Tool/software: WEBENCH® Design Tools
This is a related question that I am doing or conducting research on for a project I am working on when the forward current through a certain germanium junction diode in 20mA, the voltage drop across the diode is 0.15 volts. If the current through the diode is doubled to 40 mA, the voltage drop across the diode will be: 1) less than 0.15 volts; 2) approximately 0.15 volts; 3) between 0.15 and 0.3 volts; 4) exactly 0.3 volts.