Hello. I would like to know more how I should get a PGA (Programmable Gain Amplifier) to work with my CT (Current Transformer) (Cuttof Frequency of system: 1Khz, so i just need pga for a 2khz bandwitch or 1khz its ok) . Im developing a new design product in my company to measure current and need to interface it using an ADC (ADS1115). I would like to know part numbers and how I should get in touch with specialists in this for any doubts and implementation. We wanna to produce over than 1000 boards and if it goes well we are going to use TI Ci, thats should be a good deal for both too.
The idea of my project is plug any kind of CTs (voltage or current output). Im going to place a shunt a fixed shunt resistor of 0.1R 10W after connector to convert in the case of CT(current output like 100A:5A) current to voltage. So if I have CT(100A:5A) for a 0.1R shunt I will have 700mV on my output. So i will need to set a gain to amplify this signal from 700mV to 2.5V for instace. My ADC range is 0-4.096V. However, if I plug CT (100A:1V) it has shunt built inside then after plug it on my circuit I will have lower voltage because parallel resistance. For instance for 100A I will get 100mV instead 1V, so I will need to amplify this signal to get 2.5V. That voltage 2.5V should be my reference for my ADC measurament as instance. So after search a little I found PGA which I saw I can interface it using SPI with my uController like my ESP-12 and set the gain. As well I will need to set offset too because my uController dont read negative voltage ... But in generall thats the system which will going to use as energy metering. IN this specific occasion I wanna measure phase current and my doubt is which PGA to select and how to interface it with my uC, adjust offset and gain. I wanna to operate up to 1kHz bandwidth... If what I said looks confuse, let me know, all I want is some help to design that system =D