Part Number: TIDA-00961
Dear Salil, Dear Hrishi, Dear Texas Instruments Team,
I have got several questions to the TIDA-00961 PFC:
1) In the schematics, there is R231, R232 and R234 all connected to the same point. I assume this is to allow different options. The values with 1M are not really used. So ZVS2 and ZVS2_2 is not used. The same with R229, 230 and R233?
2) There are two signals CT_SENSE1 and CT_SENSE2. Are they used with current transformers? In the BOM I could not see current transformers.
3) The G_AC_I is not used in software and also not in hardware. The U204 and R221 cannot influence the U207 output. Only R222 and R224 take full control.
4) In the schematic, I think the J205 is drawn incorrectly. It is mirrored some way.
5) I did not find bulk capacitors in the schematic. Did you use external bulk capacitors? Hiw much uF? Which load did you use to run the PFC? What is the maximal resistance value (lowest load) that can be used?
6) Do you have got control software that you can provide and which comes along with the TIDA-PFC? In your code, you write
//GUI support variables
// sets a limit on the amount of external GUI controls - increase as necessary
volatile int16_t *varSetTxtList[16]; //16 textbox controlled variables
Can you provide the GUI for the PFC?
7) Can you provide some pictures of your test setup of TIDA-00961?
Many thanks in advance for your reply
Best regards
Patrick