Other Parts Discussed in Thread: SM74611, UC1901-SP
Hello Daniel,
Hope you are well.
Given that the max output load current from the TIDA-070002 could be 10A, why did you choose a coupled inductor
with a secondary winding rated at 10A. If the TIDA-070002 were supplying 10A, then the average and peak inductor current will be higher.
As an example, if the output load current is 7.3A, then the average and peak secondary-winding inductor currents would be 11.6 and 13.8A respectively.
Kind Regards,
Rajan.