Part Number: PMP4308
Hello,
I miss some information on the [url=https://www.ti.com/tool/PMP4308?keyMatch=pmp4308&tisearch=Search-EN-Products]PMP4308[/url]. I'm looking for the user guide. Also, I want to know which inductor is used in this design.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PMP4308
Hello,
I miss some information on the [url=https://www.ti.com/tool/PMP4308?keyMatch=pmp4308&tisearch=Search-EN-Products]PMP4308[/url]. I'm looking for the user guide. Also, I want to know which inductor is used in this design.
Hi Stefan,
Sorry there is no user guide available, but please note that the parameters of the power module is as follows:
Vin_min (V) 48V
Vin_max (V) 56.5V
Vout_nom (V) 50V
Iout_max 20A
output power 1000W
and there are five mode for selection, Io=5A, Io=10A, Io=15A and 20A and ON/OFF respectively.
Besides, the inductance L3 used in this design is 47uH manufactured by TDK, it doesn't provide detail part number since it is customized.
Regards,
Teng