Part Number: TIDA-00176
Other Parts Discussed in Thread: THS4531A
As described in the TIDA-00176 manual page 21 (chapter 4.1.1.3) the gain of the THS4531A amplifier is set to 5 for a 1Vpp input signal. This results in a 5Vpp differential signal at the output. Because we have a 2.5 common reference and 5V power supply the outputs swings from 0-5V which should not happen.
When reading the following text:
Due to the gain of 5, a typical 1-V PP input signal leverages around 50% of the ADC full-scale range (FSR),
which results in a loss of 1-bit of precision, therefore yielding an equivalent 15-bit resolution. The lower
input voltage of 0.6 V PP will leverage around 25% of the FSR, which equals typically 14-bit resolution.
I assume that a gain of 2.5 would be the right choice. What I'm thinking wrong here?