Tool/software: Code Composer Studio
I am testing the reference TIDA-01464 and I want the spec of the components: L101, T201, T202.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I am testing the reference TIDA-01464 and I want the spec of the components: L101, T201, T202.
Hello Nizar,
If you look on the TIDA-01464, at the bottom of the page you can find the BOM and Gerber files. Here is the link to the BOM (LINK: http://www.ti.com/lit/df/tidrtp7/tidrtp7.pdf). In the BOM you can find the description for each of the components for the TIDA-01464.
I have put the parts that you are looking here:
L101: Minntronix 1.6 mH, 4.3A, 0.525 ohm, TH
T201: Minntronix Transformer, 600 uH, TH
T202: Minntronix Transformer, 1500 uH, TH
Thank you
Albert Lo
Dear Albert,
I need the datatsheet of these components (core, ratio turns, ....) and is not the characteristics mentioned in the BOM. I visited the website of Minntronix but I did not find the datasheets.
Best Regards,
Nizar Sghaier.
Nizar,
Have reached out to the original designer for inductor and transformer core material specs. Some specs/calculations are already found in section 2.3.2.2 Transformer Parameter Calculations: Turns Ratio, Primary Inductance, and Peak Primary Current in the Design Guide.
Nizar,
The datasheets we have include some proprietary info. I have included excerpts in the attached.
Please reach out to Minntronix directly for more info and they will be happy to provide.MTX 4815838R.pdfMTX 4815839R.pdfMTX 4815840R.pdf