Other Parts Discussed in Thread: TPS43060, , LM293
Hello:
I'm looking into the following battery-backup reference design. However, for our application we need to support a 12V battery with a 24V Vbus / boost supply output.
I need some help in verifying that the following changes are basically what is needed. If TI can provide any guidance or help, that would be greatly appreciated.
- Modify TPS43060 output resistor FB network (for 24V)
- Modify the ULVO (EN pin) based on the 12V battery input.
- Modify transitioning circuits between boost (discharging) and buck converter (charge).
- Modify the buck converter voltage to support charging the 12V battery.
- Modify CC-CV circuit based on 12V battery votlage.