Other Parts Discussed in Thread: MSP-FET, MSP430F5172
Dear Experts,
for testing the Ultrasonic Transducer this booster pack was choose by our company.
By testing this system we was confuse, because it´s not working in the test setup.
Follow Test setup was used:
- TIDA-00462 board with external power supply 5 V
- Texas Instruments MSP-FET Flash emulation Tool
- Sharp® 96x96 Memory LCD
Now I have the problem, that the LCD are not enabled from the MSP430. For this test I use the Example Code from TI to check the functionality of the board. So, it should by work.
But LCD_BWR, LCD_SPI_CS, LCD_EN and all other pins for the LCD do nothing. The Stop LED are on after starting the system, so the MSP430 should by work.