Part Number: TIDA-01503
Hello,
the schematic of TIDA-01503 Shows that the ISO 5V is supplied from higher turns Ratio than the ISO 15V; is that correct? On sheet 1 they are connected to suitable transformer Output positions; 15V up and 5V down. However, on sheet2 the 5V is up and the 15V is down. Would you please check it? Thank you very much.
Regards,
Amr