Dear TI Experts,
I was referring TIDA-00443 Reference design from TI. TI used three 220uF capacitor C4,C5 and C18 at the output of PFC. What is the total power dissipation in these capacitor?.
TI calculated the ripple current as 2.734A in these capacitor as per the below document
http://www.ti.com/lit/ug/tidu962b/tidu962b.pdf
Regards
Aneesh