Need your help to understand P-MOSFET Q1 connection in below circuit in TIDA-00757. Here VBATT is supply and 6V is generated out of VBATT, is that correct ?
In P-FET usually source is connected to the supply side so that VGS<VT condition is met & it turns ON. Here VT is -0.85V. At t=0, VGS = 0V which isn’t less than VT so PMOS won’t turn ON. Am I missing something here ?