Other Parts Discussed in Thread: BQ25883, TUSB320LAI, TUSB320LI, TUSB320
Hello everyone,
We have designed and prototyping a board similar to PMP40496 2-cell boost charge system reference design with 5-V USB.
We have used the same schematic of this reference, but we don't use a TI microcontroller. The charge and discharge works fine, but we have a problem when connect a Power Delivery Charger (18W) through USB type-C cable. In this conditions VBUS is 0V and BQ25883 is power down.
It seem that Power Delivery charger doesn't check something and then it doesn't permits to delivery power on USB type-C cable.
What is the task of the IC TUSB320LAI in this design? Could it be a problem due to the fact that we have not implemented the microcontroller firmware?
Thank you for the support!
Best Regards,