Other Parts Discussed in Thread: PMP10833, PMP20122
Hi,
I'm thinking about using the same circuit as the one presented in your board PMP10834 for my design that needs an AC/DC with 5V output (max 0.5A).
To save space and costs, since I don't need a high precision on the 5V (il will just be used as input for simple DC/DC), I'm thinking about using just a resistor divider for the feedback signal (similar to PMP10833).
My question is: the GND of component UCC28C45D is the voltage between the sense resistor and the inductor. Shall this same voltage be the "GND" for the resistor divider for the feedback voltage (like your design PMP10833) ?
If so, I don't understand how UCC28C45D can sense the correct voltage, since (at DC) the voltage at the output of the inductor is the same as the voltage at the input of the inductor (the GND of component UCC28C45D). The output of the voltage divider would give 0V instead of the correct voltage for UCC28C45D to work properly.
Where am I wrong ?
Thanks a lot for your help !
Luca.