Tool/software: Code Composer Studio
Hey guys,
in the Sub 1GHz forum, I was asked to check the Tx frequency accuracy of our TIDA board, since we had issues with the caps of our 32kHz crystal. We used different transmission modes (SmartRF Studio) and used continuous Tx with unmodulated transmission. We compared the results of a CC1352R1 launchpad to ours. The device for signal acquisition was a LeCroy oscilloscope with 10GS/s samplerate, the measured frequency was the average of some tens to hundreds of thousand measurement points (one point included around 50 periods of the sub GHz sine) Here are the results:
Do we have to adjust the cap array or are we good enough for certification? (ETSI + FCC)
best wishes
Slev1n