Other Parts Discussed in Thread: UCC28700
Tool/software: WEBENCH® Design Tools
Hello all,
I am currently developing a 24V@1A DC power supply using UCC28631DR. For the initial design i used Webench, but couldn't find am off-the-shelf transformer. So I had to replace with the Coilcraft's JA4429-AL, That was the closest one I could find with the parameters given at Webench. I have adapted the voltage reference resistor that feed VSENSE to fit the turns ratio of the used transformer.
My question is if JA4429-AL would be a suitable replacment to work with UCC28631DR and, if there's any other modification that has to be made on the system aside from the VSENSE resistors.
The Webench design can be found at webench.ti.com/.../SDP.cgi
EDIT: I have attached the schematics of the converterUCC28631_converter.pdf
Thank you for the support.