This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62177: TPS62177DQCR Error power good signal

Part Number: TPS62177


Hello, I am having trouble with TPS62177


Input voltage 12V, output 3.3V, R12 not soldered. And although the output voltage is 3.309V there is no PG signal. The voltage on the PG (7) leg is 3.3V and the transistor VT1 is closed. This is tested on more than 10 chips and the effect is repeated.

Why could this be?