Part Number: TIDA-010032
Hello,
I can't seem to find information regarding the dimensions of the entire design.
I'm also looking for examples for typical power consumption of the board while the processor is active.
Thank you in advanced,
Daniel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-010032
Hello,
I can't seem to find information regarding the dimensions of the entire design.
I'm also looking for examples for typical power consumption of the board while the processor is active.
Thank you in advanced,
Daniel
Hi Daniel,
Dimension of the overall design which includes docking board, BeagleBone Black (AM335x), and CC1312R1 launchpad is 5.9" (inch) x 5.9" (inch). This reference design implements universal data concentrator providing a complete IPv6- based network solution integrated with Ethernet backbone communication, 6LoWPAN RF mesh networking, RS-485. However, this may not be completely optimized for the size since it uses two standard launchpads for the demonstration purpose.
Power consumption of individual launchpads depends on the features that are being enabled. We do not have the overall power consumption data taken for the data concentrator setup.
With Regards,