Hi,
i accedently stopted the Jtag while it was burn the firmware and now i get this error messege:
"C28xx: Error connecting to the target: (Error -1015 @ 0x0) Device is not responding to the request. Device may be locked, or the debug probe connection may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board). If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006)
"
i assume that Device is locked,
How can i reopend it?
Thanks,
Michael