Hi,
i want to examine the circuit manually by insert a voltage to the adc inputs. J5 pins 1,2,4,10 etc..
what is the current limit for that signals?
and the voltage is 0 to 3.3 V ?
thanks,
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
i want to examine the circuit manually by insert a voltage to the adc inputs. J5 pins 1,2,4,10 etc..
what is the current limit for that signals?
and the voltage is 0 to 3.3 V ?
thanks,
Michael
Hi Micheal
the drive current for ADC input is very small, you could limit the current to 1mA for each ADC channel.
ADC input voltage range should be 0V~3.3V.