This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP10948: 300V output with 4A max load

Part Number: PMP10948

Hello, I am a student with basic smps knowledge. I want to know if PMP10948 can be modified to set output voltage to 300V with 4A load capacity. It would be helpful if anyone can point out which component needs to be modified and the reason behind it.

Thanks