Other Parts Discussed in Thread: INA260, INA226-Q1, INA239-Q1
Hi,
I am developing an application to measure the current from a 12V Vehicle battery in different load conditions,
the voltage will be in between +11 V to 13V maximum ut the load may vary from 10W to 500W
I would like to use the above reference for the same the load current may vary up to 10A max so can I use the above TIDA-01608 reference to measure the power?
or is there an alternative reference for the same?
Please provide your feedback ASAP
With Regards,
Rakesh hegden M N