Other Parts Discussed in Thread: TPS55340-Q1, , TPS55340
Hello Team,
Good day.
My Customer wanted to use the TPS55340-Q1, checking the TIDA-01323 this has a schematic available with TPS55340-Q1 that fits his need (Vin 4 - 40V). However, upon checking the device datasheet the max recommended input of TPS55340-Q1 is 38V, can you confirm the schematic of TIDA-01323 is correct and can be followed? even the input is 4- 40V for TPS55340-Q1?
TIDA-01323 SchematicLink: https://www.ti.com/lit/df/tidrtr6/tidrtr6.pdf
Regards,
_Renan