Hello team,
Is there side photo of PMP5711? I would like to confirm component height.
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
Is there side photo of PMP5711? I would like to confirm component height.
Best regards,
Hello Taketo-san,
attached the side view of my converter; max. height is dominated by input capacitor size H13,
height 13.5mm, and transformer Payton #55880, here height is <15mm.
I made this design almost a decade ago, would go towards newer FETs and would replace input
capacitor by Panasonic hybrid 2x 47uF/80V ZC series.
Attached the stress analysis at nominal input 48V; at full load 35A the supply needs forced cooling.
Best regards, Bernd