This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61175-Q1: Review of switchable output voltage design

Part Number: TPS61175-Q1

Hi,

I have taken TPS61175-Q1 and made 2 designs. One with output of 12V and one with 24V.

In my board Ill be switching the output voltage between 12V and 24V by putting a resistor in parallel with one of the feedback resistor. The resistor in parallel would be connected to a switch for switchable output voltage control.

Is this possible to achieve by keeping all the components same for both designs except the feedback resistors?

Attached are the reports for both designs for review

24V 120mA 85C TPS61175Q1.pdf

12V 120mA 85C TPS61175Q1.pdf