The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01486: Overheating design - need clarification

Part Number: TIDA-01486
Other Parts Discussed in Thread: THS3095

Hi,

My customer just received their newly built TIDA-01486 AFE board and smelled 'hot components'.

When large signals pass the RX portion, the 10ohm resistors R39-R42 may source up to an Ampere into the protective diodes, and the amplifier THS3095 gets blazing hot.

Question: - Why are R39-R42 not 100ohm or larger? Was it a typo and should have been 10kohm instead?

We cannot get our heads around the selection criteria of 10ohms in those positions.

Please clarify a.s.a.p.

Thanks.

B.r M.A.M