Other Parts Discussed in Thread: TPS40210-Q1, TPS40210
Hello
I have Inquiry of Fly-Back circuit in TIDA-00281.
1. What is the maximum output current of a fly-back circuit using TPS40210-Q1 in TIDA-00281?
2. Could you provide a PSPICE file for the fly-back circuit below?
3. Could you provide a reference design if the output is 0.5A at 12V?
Best regards.