Other Parts Discussed in Thread: UCC21530, UCC21520
Tool/software: WEBENCH® Design Tools
Hi,
I am using a UCC21530 driver for generating a gate pulse. At the input enable pin, I have given a 2.3V supply with a voltage divider from 5V input. But I am getting the gate output voltage as constant and negative, same as the Vsa and Vsb (Pin no 14,9).
All the input pins are correctly showing the expected voltage values including the pulse input. The output biasing supplies are also showing +15V and -5V at the desired pins. But the gate outputs at HO and LO are showing the fixed negative voltage of -5V. (Vsa and gate outputs aren't sorted) I am not able to find the reason. Please sort out the problem if possible. I like to mention that I am testing only the gate driver without any load or switch connection, only with two isolated biasing voltage supplies and some coupling capacitors.
Thank you for your valuable time.