Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM46002: LM46002 TINA simulation for -12V/1.5A

Part Number: LM46002

Tool/software: WEBENCH® Design Tools

Hi,

I'm trying to do transient analysis using TINA. Can you please let me know if any fix is required in snvm606.tsc file?

Attachment: snvm606.tsc

Design specifications:

Input voltage: 24V

Output voltage: -12V

Output current: 1.5A

snvm606.tsc