Hi,
I'm working on a PFC based on the eval kit TIDA-00779. Made a new PCB for that.
Now I found out, that in schematic and BOM the value of C14 is 8.2uF ..... but the given PN
out of the BOM is pointing to a 4.7uF device.
Out of the BOM:
C14 = CAP, CERM, 8.2 μF, 25 V, +/- 10%, X5R, 0603 AVX 0603ZD475KAT2A
C14 is used for compensation, so I think it's important to know what value is correct.
Thanks and have a good day
Pepito