The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00951: Firmware or Flow chart of MCU

Part Number: TIDA-00951

Hi,

TIDA-00951 main board prototype has been manufactured with gerber file supplied on the TI web page. I will get PCB prototypes of  TIDA-01141 Currrent Measurement Module, TIDA-01159 Gate Drive Module, and TIDA-01281 Communication Module soon. But I can not go forward because i have not firmware for TIDA-01281 Communication Module. I have requested the firmware from TI a couple of times, but i have not received an approval message from them yet. I can not understand why they do not approve it. I have been using TI' s battery management ICs, Li-Ion charger ICs, evaluation modules, mosfets, software etc since 2007.

I have a couple of questions about TIDA 00951,

1) Does the combination of the TIDA-00951 and TIDA-01141 and TIDA-01159 work properly? (without TIDA-01281 Communication Module).  Or is there any way to operate it somehow?

2) If the firmware for TIDA-01281 is not supplied from TI, is it available to get flow chart of TMS320F28033 MCU? Because developing our own software would be second way to complete project.

Best rgerads,

Yusuf Kaya