Hi,
I have installed Pspice for Ti. I have following Problems:
1) There is no start menu entry 2) I can find capture.exe at C:\Cadence\PSpiceTI\tools\bin, but I can run that only as admin. 3) If I open capture.exe normally it throws a error. 4) there is no uninstall file in control panel.
I have seen similar problems in the thread, and the TI engineer asked few questions. Am answering them below:
1. Is the issue that you have installed the tool, and after installation you are not able to see the tool entry in Windows programs?
Ans: Yes
2. Do you see a folder at C:\Cadence\PSpiceTI\tools\bin that contains capture.exe?
Ans:Yes, I see capture.exe at C:\Cadence\PSpiceTI\tools\bin
3. Were you logged in as the admin account or the non-admin account?
Ans: I logged in as non-admin account
4.2, If you logged in using a non-admin account, did you right click on PSpice-For-TI_setup.exe and selected Run as administrator and entered the admin account's credentials?
Yes, our IT engineer installed Pspice-for-Ti with admin privilege's. Which I don't have.
Hope I answered all questions in advance :D. Is there a solution to this problem ?
Br
Ravi Kiran