hi everyone!
good day !
I am working with TMDSHVMTRSPIN v2.1 and Lab03a for both control cards.
I insert the F28027F control card and run a motor ..after loading motor the Trip signal (TZ-1) got active but the motor did not stop!
I have done the same action with F28069M control card and motor stop due to fault current| signal (TZ-1). it worked properly.
so , I could not figure out why is that !
Q1: is that something normal and all of the F28027F control card TZ-1 are disabled ?(or mine has problem)?
Q2: how to active the TZ-1 signal for F28027F in lab 3a?
thanks for attention .
Dave.