Hi
Please refer to Fig. 38.
I wish to know the input supply of 17V to TPS82130SILR was taken from a separate source. If yes, how please?
Precisely, I am designing a two stage converter with an input rectifier (stage 1) having 230V input voltage and output voltage of 400Vdc. The 400Vdc serves as a Dc link voltage that powers the second stage (dual active bridge converter). Now I wish to provide an input voltage of 17 V to TPS82130SILR within the system not from an external source. Kindly advise.
Regards,
Olutayo.