Part Number: TIDA-00637
Tool/software: Code Composer Studio
Hi Team,
The customer has a question about TIDA-00637 schematic for the isolation/application question as below? Could you help check it? Thank you.
The Line and Neutral after resister divider then connect to MCU pin1 & pin2. However, we can't find the connection between R18 and R20.
Which ground should it connect? Or due to MCU just want to get the differential signal of AC voltage, so it didn't need to connect to any gnd? (Pic1)
Also, the primary side of V1/V2 connect to secondary side of V1+/V1- without the isolation, will there be any issue? Can this application meet the primary to secondary Hi-Pot testing?
Best regards,
Mike