Part Number: TIDA-00951
Hi,
I am using Tıda-00951 2-kW, 48- to 400-V,Isolated Bidirectional DC-DC Converter with Tıda -00951 software, programming of the control card with the appropriate software.
I am using the tida-01281 board as the control card and tıda-01141, tida-01159 HV mosfet driver and current sensing.
After assembling all the cards I applied 36 volts to the battery input (J9, J 11) and I applied a 12-V auxiliary supply to connector J6. As soon as I turn on the power, the side of LV mosfet driver U8 is burned.
I was not applied VBUS voltage , and I am nat using electronik load.
Do I need to make a change through the software.
How can ı test of mosfet driver pwm signal, how shoud be pwm signal.