Hi Team,
Our customer would like to know if it is possible to use the TIDA-00254 with the BlackFly S Series from Flir and which camera specifications are necessary to use with the Reference HW.
Regards,
Danilo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Our customer would like to know if it is possible to use the TIDA-00254 with the BlackFly S Series from Flir and which camera specifications are necessary to use with the Reference HW.
Regards,
Danilo
Hello Danilo,
Welcome back to the E2E forum!
Is your client considering using the BlackFly S as a replacement for the EVM's optical module or in parallel with it?
Regards,
Austin
Danilo,
Per the User's Guide:
"Each projected pattern is captured by the Point Grey Flea3 global or rolling shutter camera or a compatible Open CV camera (such as a webcam)."
So, as long as the camera you are using is OpenCV compatible you should be OK. I don't believe that the team has tested this platform with this particular camera, but it looks like it was developed by the same company.
I would note that the resolution for the camera you are looking at is lower, however. So performance may not be the same as the recommended camera.
I hope this helps.
Regards,
Philippe Dollo