Hello,
We have a TIDA-020032 board sample from TI which we are trying to flash using XDS110. We connected the board with debugger probe & when we try to run one of examples as in the associated Simple Link SDK, we get this error
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
Cortex_M3_0: Command=20 -- addr=0x00002000 -- length=0x00001000
Cortex_M3_0: File Loader: Memory write failed: Timed out waiting for target flashloader to execute command.
Cortex_M3_0: GEL: File: C:\Users\premkiran.slnrm\workspace_v10\ble5_host_test_cc2640r2lp_app\FlashROM_StackLibrary\ble5_host_test_cc2640r2lp_app.out: Load failed.
We checked the JTAG is correct. Are we missing anything here?
Also please let us know the settings in CCS using XDS110 to build and flash the board with any examples provided.
Regards
Prem