This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP20612: Rerence design PMP20612 and TIDA-01464 thermal map differences

Part Number: PMP20612
Other Parts Discussed in Thread: TIDA-01464

Hello !
Why reference design PMP20612 and TIDA-01464 have such HUGE difference (about 2 times) in thermal map at 230Vac full load ?
Schematic are the same, BOMs are identical.

BR, Grigory

  • Hi,

    Yes, TIDA-01464 uses the same hardware. I captured PMP20612 thermal image at least 30mins after I power up the board with 200W load. But it is unclear how long did the thermal image captured after the board is powered up.

    Regards,

    Sheng-Yang Yu