Other Parts Discussed in Thread: ASH
#1 -- From the reference design, I see the RC snubber to be one of the main contribution for the source of power loss/heat. Is there an option to change the values for RC to reduce power/thermals? What is the impact in the system design?
#2 -- The parametric table shows 12V, 4.25A as output while the Test data show only 12V, 3.7A as the output which is confusing. Should we assume 51W for the load or 44.4W at the load with 6.7W in losses?
Thanks,
Ash