How much the phase difference of PWM signal between half bridge 1 and 2?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
It is 180 degrees.
Regards,
Salil
I need to shift the PWM frequency too. I plan to shift them by hardware, do you have any suggest?
I use STM32F4 series MCU to control the gate driver
Hi Khyarul,
Changing the frequency through hardware is much more difficult than doing so through firmware. I don't understand why you need to do so.
Regards.
Salil
If I set the first's PWM duty cycle to 70% and the second's PWM duty cycle must be 70% too?
What if I set them both 100%? Is it safe?
Yes, the duty cycles of both the phases should be the same for current balancing.
Since the gate driver in TIDA-00120 requires bootstrap bias for the high side MOSFET, you can't get 100% duty cycle operation. The maximum duty cycle has to be limited to around 95% to allow sufficient time for the bootstrap to charge.
Regards,
Salil