Other Parts Discussed in Thread: BQEVSW
I am having issues with programming the EEPROM on the bq27x10EVM when interfaced with the EV2400 board. the data is not getting persisted when I write to EEPROM. I am connected out of the PORT3 HDQ to the bq27x10EVM board the Communication Status shows OK.
so when connected from Port3 (HDQ) of EV2400 to the bq27X10 board the communication status is OK.
when I try to go to the EEPROM tab and change the value of Initial LMD from 44 to 63 it does not persist after I write the values to EEPROM. see attached image
Also on one of my windows 10 computer, I am getting the following error,it is not allowing me to uninstall it - bq27x10 single-cell battery gas gauge. see an attached error message.
after the application starts, I get the error message and when I close the error message by pressing ok the application closes too. also, i tried to uninstall the program it does not allow me to do so. it gives the following error message