Part Number: TIDA-00929
Other Parts Discussed in Thread: AFE3010,
Hi!
I am planning to design the residential circuits breaker with both arc fault and ground fault circuits interrupt. Which reference design will fit both requirements?
I would like to have input range up to 360VAC and current limit up to 70A. Please also include the WiFi and eithernet chipsets as well.
If possible, could it possible to have an AE to set up a conference call?