Other Parts Discussed in Thread: CC2652RB, CC2640R2F, CC2642R, SYSCONFIG
HI,
I always see these parameters set at CC2640R2F Simple Peripheral. However, at CC2652RB simple peripheral, I can not find where these parameters are set. I can not find it at syscfg.
// Minimum connection interval (units of 1.25ms, 80=100ms) for automatic // parameter update request #define DEFAULT_DESIRED_MIN_CONN_INTERVAL 80 // Maximum connection interval (units of 1.25ms, 800=1000ms) for automatic // parameter update request #define DEFAULT_DESIRED_MAX_CONN_INTERVAL 800 // Slave latency to use for automatic parameter update request #define DEFAULT_DESIRED_SLAVE_LATENCY 0
-kel