Other Parts Discussed in Thread: CC1352R, CC1310
Hello Everyone,
I am Piyush Saxena,
I have a requirement where clients wants to have atleast 6 sub ghz wireless switch to be connected simultaneously with the a central hub. The central Hub should have bluetooth (for monitoring the wireless switch status on mobile application) and sub ghz for wireless connection with the wireless switch.
After doing some research I have came across a solution i.e. using CC1310 for wireless switch and using CC1352R/P for the central hub. Whereas since I do not have prior experience working with these MCU hence I have some queries mentioned below.
It will be great if someone can help me with the following queries.
I would like to have a confirmation if 6 Sub Ghz CC1310 can be simultaneous connected with the CC1352R/P MCU?
Since CC1352R/P is a multiprotocol MCU hence can you please let me know what is the maximum number of CC1310 that can be connected to CC1352R/P. Also please let me know if we can also used the bluetooth feature simultaneously. If yes then what shall be the possible data rate I should expect for the bluetooth connection.
Also please let me know the impact on Flash and Ram of the Central hub i.e. CC1352 on adding each wireless switch.
Thank you.