Other Parts Discussed in Thread: SYSCONFIG
Hello
I'm hoping someone will be able to help me with a linker error I've recently come across.
It recently happened after adding files related to a compiled Sensor Controller project but I'm unsure on how the error is related. The linker error is as follows;
Description Resource Path Location Type
#16004-D file "C:/ti/simplelink_cc13x2_26x2_sdk_5_10_00_48/source/ti/display/lib/ccs/m4f/display.a<LCDDogm1286_util.oem4f>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files dsb_app_fw C/C++ Problem
I can work around this by disabling the Display TI driver in the SysConfig, but ideally I'd like to understand what is happening.
If I work backwards in my commit history around at the same time the following automated changes are made to the "src/makefile.libs" as well as a whole bunch of changes to the .cproject file is when the linker error occurs. Being as it seems to be a floating point related linker error and the 'f' being dropped from the makefile seems to suggest something has happened, but I'm not sure what.
Any help is appreciated.
Nicholas