Other Parts Discussed in Thread: UNIFLASH, SEGGER, CC1352R
Setup:
SDK: simplelink_cc13x2_26x2_sdk_5_10_00_48
Compiler: CCS Compiler
Uniflash: 6.3.0.3193
Programmer: TI CC1352R LAUNCHXL and Segger
Devices: Two CC1352R LPSTK revision E
Bootlaoder: bim_offchip_CC1352R1_LAUNCHXL_nortos_ccs
Application: simple_peripheral_oad_offchip_CC13X2R1_LAUNCHXL_tirtos_ccs
Hi Experts,
I am facing some issues while flashing binary with both Uniflash and Jlink.
Without any modification, I built bim_offchip bootloader and simple_peripheral_oad_offchip examples.
Test 1:
With Uniflash, if I sequentially flash the bootloader (*.hex) and then the simple_peripheral_oad_offchip (*.out).
[Works as intended] After the program load, the device reboots by itself, and launches the simple_peripheral_oad_offchip firmware without any manual action.
6/10/2021, 11:01:19 AM] [INFO] Cortex_M3_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:01:24 AM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:01:24 AM] [INFO] Cortex_M4_0: Flashloader: Verbose output enabled. [6/10/2021, 11:01:26 AM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:01:26 AM] [INFO] Cortex_M4_0: GEL Output: Board Reset Complete. [6/10/2021, 11:01:26 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00056000 of Length 0x00001138 [6/10/2021, 11:01:26 AM] [INFO] Cortex_M4_0: Performing bank erase [6/10/2021, 11:01:26 AM] [INFO] Cortex_M4_0: Loading flashloader to target: FlashLoaderCC26x2.out [6/10/2021, 11:01:27 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00056000, length=4408, crc=0x738EB07D (using block 1) [6/10/2021, 11:01:27 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00057fa8 of Length 0x00000058 [6/10/2021, 11:01:27 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00057FA8, length=88, crc=0xB0D43234 (using block 0) [6/10/2021, 11:01:28 AM] [SUCCESS] Program Load completed successfully. [6/10/2021, 11:01:48 AM] [INFO] Cortex_M3_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:01:53 AM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:01:53 AM] [INFO] Cortex_M4_0: Flashloader: Verbose output enabled. [6/10/2021, 11:01:55 AM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:01:55 AM] [INFO] Cortex_M4_0: GEL Output: Board Reset Complete. [6/10/2021, 11:01:55 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00000000 of Length 0x00007ff0 [6/10/2021, 11:01:55 AM] [INFO] Cortex_M4_0: Loading flashloader to target: FlashLoaderCC26x2.out [6/10/2021, 11:01:55 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00000000, length=8192, crc=0x0BC95FEA (using block 0) [6/10/2021, 11:01:56 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x00002000, length=8192, crc=0x02DA14AB (using block 1) [6/10/2021, 11:01:56 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x00004000, length=8192, crc=0x242B801E (using block 0) [6/10/2021, 11:01:56 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x00006000, length=8176, crc=0x11143C29 (using block 1) [6/10/2021, 11:01:56 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00007ff0 of Length 0x00007ff0 [6/10/2021, 11:01:56 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00007FF0, length=8192, crc=0x69B4779B (using block 0) [6/10/2021, 11:01:57 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x00009FF0, length=8192, crc=0x03D704E9 (using block 1) [6/10/2021, 11:01:57 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x0000BFF0, length=8192, crc=0xF1889C83 (using block 0) [6/10/2021, 11:01:57 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x0000DFF0, length=8176, crc=0x5F427E11 (using block 1) [6/10/2021, 11:01:57 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x0000ffe0 of Length 0x00007ff0 [6/10/2021, 11:01:57 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x0000FFE0, length=8192, crc=0xB4CAB77D (using block 0) [6/10/2021, 11:01:58 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x00011FE0, length=8192, crc=0xB4E60C97 (using block 1) [6/10/2021, 11:01:58 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x00013FE0, length=8192, crc=0xAE6347E2 (using block 0) [6/10/2021, 11:01:58 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x00015FE0, length=8176, crc=0x05A6EA1F (using block 1) [6/10/2021, 11:01:58 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00017fd0 of Length 0x00006630 [6/10/2021, 11:01:58 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00017FD0, length=8192, crc=0x7EB8797F (using block 0) [6/10/2021, 11:01:58 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x00019FD0, length=8192, crc=0x731E740C (using block 1) [6/10/2021, 11:01:59 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x0001BFD0, length=8192, crc=0xFB155709 (using block 0) [6/10/2021, 11:01:59 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x0001DFD0, length=1584, crc=0xB8CDB500 (using block 1) [6/10/2021, 11:02:00 AM] [SUCCESS] Program Load completed successfully.
Test 2:
With Uniflash, if I sequentially flash the bootloader (*.hex) and then the simple_peripheral_oad_offchip (*.hex):
[Does not work as intended] After the program load, the device does not reboot automatically.
- After the 1st power cycle: nothing happen.
- After the 2nd power cycle: the recovery image Multi-Sensor is launching instead of the application.
6/10/2021, 11:07:52 AM] [INFO] Cortex_M3_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:07:57 AM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:07:57 AM] [INFO] Cortex_M4_0: Flashloader: Verbose output enabled. [6/10/2021, 11:07:59 AM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:07:59 AM] [INFO] Cortex_M4_0: GEL Output: Board Reset Complete. [6/10/2021, 11:07:59 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00056000 of Length 0x00001138 [6/10/2021, 11:07:59 AM] [INFO] Cortex_M4_0: Performing bank erase [6/10/2021, 11:07:59 AM] [INFO] Cortex_M4_0: Loading flashloader to target: FlashLoaderCC26x2.out [6/10/2021, 11:07:59 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00056000, length=4408, crc=0x738EB07D (using block 1) [6/10/2021, 11:07:59 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00057fa8 of Length 0x00000058 [6/10/2021, 11:07:59 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00057FA8, length=88, crc=0xB0D43234 (using block 0) [6/10/2021, 11:08:00 AM] [SUCCESS] Program Load completed successfully. [6/10/2021, 11:08:13 AM] [INFO] Cortex_M3_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:08:18 AM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:08:18 AM] [INFO] Cortex_M4_0: Flashloader: Verbose output enabled. [6/10/2021, 11:08:20 AM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 11:08:20 AM] [INFO] Cortex_M4_0: GEL Output: Board Reset Complete. [6/10/2021, 11:08:22 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00000000 of Length 0x0000008d [6/10/2021, 11:08:22 AM] [INFO] Cortex_M4_0: Loading flashloader to target: FlashLoaderCC26x2.out [6/10/2021, 11:08:22 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00000000, length=141, crc=0xD3F58142 (using block 0) [6/10/2021, 11:08:22 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00000090 of Length 0x0000003c [6/10/2021, 11:08:22 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00000090, length=60, crc=0xCA5AED48 (using block 1) [6/10/2021, 11:08:22 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x000000d0 of Length 0x00007ff0 [6/10/2021, 11:08:22 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x000000D0, length=8192, crc=0x9CF69E46 (using block 0) [6/10/2021, 11:08:23 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x000020D0, length=8192, crc=0xBCFE35F8 (using block 1) [6/10/2021, 11:08:23 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x000040D0, length=8192, crc=0x6E83A2F6 (using block 0) [6/10/2021, 11:08:23 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x000060D0, length=8176, crc=0x2BA9892E (using block 1) [6/10/2021, 11:08:23 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x000080c0 of Length 0x00007ff0 [6/10/2021, 11:08:24 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x000080C0, length=8192, crc=0x76FFD0FF (using block 0) [6/10/2021, 11:08:24 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x0000A0C0, length=8192, crc=0x90FE2B0D (using block 1) [6/10/2021, 11:08:24 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x0000C0C0, length=8192, crc=0xC26933C7 (using block 0) [6/10/2021, 11:08:24 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x0000E0C0, length=8176, crc=0x0833A055 (using block 1) [6/10/2021, 11:08:24 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x000100b0 of Length 0x00007ff0 [6/10/2021, 11:08:25 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x000100B0, length=8192, crc=0x948018DC (using block 0) [6/10/2021, 11:08:25 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x000120B0, length=8192, crc=0x6E149376 (using block 1) [6/10/2021, 11:08:25 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x000140B0, length=8192, crc=0x14517B08 (using block 0) [6/10/2021, 11:08:25 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x000160B0, length=8176, crc=0xCA3A7616 (using block 1) [6/10/2021, 11:08:25 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x000180a0 of Length 0x00007ff0 [6/10/2021, 11:08:26 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x000180A0, length=8192, crc=0xF4637A47 (using block 0) [6/10/2021, 11:08:26 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x0001A0A0, length=8192, crc=0xB21C5EDB (using block 1) [6/10/2021, 11:08:26 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x0001C0A0, length=8192, crc=0xA6AEB2EC (using block 0) [6/10/2021, 11:08:26 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x0001E0A0, length=8176, crc=0x70DBF215 (using block 1) [6/10/2021, 11:08:26 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00020090 of Length 0x00001420 [6/10/2021, 11:08:27 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00020090, length=5152, crc=0x56A28BCB (using block 0) [6/10/2021, 11:08:27 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x000214b0 of Length 0x00000aa0 [6/10/2021, 11:08:27 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x000214B0, length=2720, crc=0xF68FCB1E (using block 1) [6/10/2021, 11:08:28 AM] [SUCCESS] Program Load completed successfully.
Test 3:
With Uniflash, if I select both images for flashing the bootloader (*.hex) and simple_peripheral_oad_offchip (*.out):
[Does not work as intended] After the program load, the device does not reboot automatically.
- After the 1st power cycle (by removing the programmer): nothing happens.
- After the 2nd power cycle (by removing the programmer): the recovery image is launching instead of the application.
[6/10/2021, 10:34:53 AM] [INFO] Cortex_M3_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 10:34:58 AM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 10:34:58 AM] [INFO] Cortex_M4_0: Flashloader: Verbose output enabled. [6/10/2021, 10:35:00 AM] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete. [6/10/2021, 10:35:00 AM] [INFO] Cortex_M4_0: GEL Output: Board Reset Complete. [6/10/2021, 10:35:00 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00000000 of Length 0x00007ff0 [6/10/2021, 10:35:00 AM] [INFO] Cortex_M4_0: Performing bank erase [6/10/2021, 10:35:00 AM] [INFO] Cortex_M4_0: Loading flashloader to target: FlashLoaderCC26x2.out [6/10/2021, 10:35:01 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00000000, length=8192, crc=0x0BC95FEA (using block 1) [6/10/2021, 10:35:01 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x00002000, length=8192, crc=0x02DA14AB (using block 0) [6/10/2021, 10:35:01 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x00004000, length=8192, crc=0x242B801E (using block 1) [6/10/2021, 10:35:02 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x00006000, length=8176, crc=0x11143C29 (using block 0) [6/10/2021, 10:35:02 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00007ff0 of Length 0x00007ff0 [6/10/2021, 10:35:02 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00007FF0, length=8192, crc=0x69B4779B (using block 1) [6/10/2021, 10:35:02 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x00009FF0, length=8192, crc=0x03D704E9 (using block 0) [6/10/2021, 10:35:03 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x0000BFF0, length=8192, crc=0xF1889C83 (using block 1) [6/10/2021, 10:35:03 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x0000DFF0, length=8176, crc=0x5F427E11 (using block 0) [6/10/2021, 10:35:03 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x0000ffe0 of Length 0x00007ff0 [6/10/2021, 10:35:03 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x0000FFE0, length=8192, crc=0xB4CAB77D (using block 1) [6/10/2021, 10:35:03 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x00011FE0, length=8192, crc=0xB4E60C97 (using block 0) [6/10/2021, 10:35:03 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x00013FE0, length=8192, crc=0xAE6347E2 (using block 1) [6/10/2021, 10:35:04 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x00015FE0, length=8176, crc=0x05A6EA1F (using block 0) [6/10/2021, 10:35:04 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00017fd0 of Length 0x00006630 [6/10/2021, 10:35:04 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00017FD0, length=8192, crc=0x7EB8797F (using block 1) [6/10/2021, 10:35:04 AM] [INFO] Cortex_M4_0: Chunk 2: addr=0x00019FD0, length=8192, crc=0x731E740C (using block 0) [6/10/2021, 10:35:05 AM] [INFO] Cortex_M4_0: Chunk 3: addr=0x0001BFD0, length=8192, crc=0xFB155709 (using block 1) [6/10/2021, 10:35:05 AM] [INFO] Cortex_M4_0: Chunk 4: addr=0x0001DFD0, length=1584, crc=0xB8CDB500 (using block 0) [6/10/2021, 10:35:05 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00056000 of Length 0x00001138 [6/10/2021, 10:35:05 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00056000, length=4408, crc=0x738EB07D (using block 1) [6/10/2021, 10:35:05 AM] [INFO] Cortex_M4_0: Writing Flash @ Address 0x00057fa8 of Length 0x00000058 [6/10/2021, 10:35:05 AM] [INFO] Cortex_M4_0: Chunk 1: addr=0x00057FA8, length=88, crc=0xB0D43234 (using block 0) [6/10/2021, 10:35:06 AM] [SUCCESS] Program Load completed successfully.
Test 4:
Since Jlink does not support the *.out format, I flash the device with both the bootloader (*.hex) and then the simple_peripheral_oad_offchip (*.hex).
[Does not work as intended] The device boots the recovery image "Multi-Sensor".
'C:\Program Files (x86)\SEGGER\JLink\JLink.exe' -device cc1352R1F3 -if jtag -speed 4000 -jtagconf -1,-1 -autoconnect 1 -CommandFile .\cmd.jlink SEGGER J-Link Commander V6.98c (Compiled Mar 16 2021 12:20:44) DLL version V6.98c, compiled Mar 16 2021 12:19:26 J-Link Command File read successfully. Processing script file... J-Link connection not established yet but required for command. Connecting to J-Link via USB...O.K. Firmware: J-Link V10 compiled Feb 4 2021 12:58:41 Hardware version: V10.10 S/N: 50114253 License(s): GDB VTref=3.216V Target connection not established yet but required for command. Device "CC1352R1F3" selected. Connecting to target via JTAG InitTarget: Found ICE-Pick with ID: 0x3BB4102F InitTarget: Found CPU TAP 0x4BA00477 DPv0 detected Scanning AP map to find all available APs AP[1]: Stopped AP scan as end of AP map has been reached AP[0]: AHB-AP (IDR: 0x24770011) Iterating through AP map to find AHB-AP to use AP[0]: Core found AP[0]: AHB-AP ROM base: 0xE00FF000 CPUID register: 0x410FC241. Implementer code: 0x41 (ARM) Found Cortex-M4 r0p1, Little endian. FPUnit: 6 code (BP) slots and 2 literal slots CoreSight components: ROMTbl[0] @ E00FF000 ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7 ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM ROMTbl[0][4]: E0040000, CID: B105900D, PID: 000BB9A1 TPIU Cortex-M4 identified. PC = 1000060A, CycleCnt = 00240DBC R0 = 00000004, R1 = 40082000, R2 = 00000000, R3 = 00000000 R4 = E000ED10, R5 = 00000004, R6 = FFFFFFFF, R7 = FFFFFFFF R8 = 10000000, R9 = FFFFFFFF, R10= FFFFFFFF, R11= FFFFFFFF R12= 00000000 SP(R13)= 20005B18, MSP= 20013FF8, PSP= 20005B18, R14(LR) = 100036C5 XPSR = 81000000: APSR = Nzcvq, EPSR = 01000000, IPSR = 000 (NoException) CFBP = 02000001, CONTROL = 02, FAULTMASK = 00, BASEPRI = 00, PRIMASK = 01 FPS0 = 00000000, FPS1 = 00000000, FPS2 = 00000000, FPS3 = 00000000 FPS4 = 00000000, FPS5 = 00000000, FPS6 = 00000000, FPS7 = 00000000 FPS8 = 00000000, FPS9 = 00000000, FPS10= 00000000, FPS11= 00000000 FPS12= 00000000, FPS13= 00000000, FPS14= 00000000, FPS15= 00000000 FPS16= FFFFFFFF, FPS17= FFFFFFFF, FPS18= FFFFFFFF, FPS19= FFFFFFFF FPS20= FFFFFFFF, FPS21= FFFFFFFF, FPS22= FFFFFFFF, FPS23= FFFFFFFF FPS24= FFFFFFFF, FPS25= FFFFFFFF, FPS26= FFFFFFFF, FPS27= FFFFFFFF FPS28= FFFFFFFF, FPS29= FFFFFFFF, FPS30= FFFFFFFF, FPS31= FFFFFFFF FPSCR= 00000000 Without any give address range, Erase Chip will be executed Erasing device... J-Link: Flash download: Total time needed: 1.186s (Prepare: 0.484s, Compare: 0.000s, Erase: 0.697s, Program: 0.000s, Verify: 0.000s, Restore: 0.004s) Erasing done. Downloading file [.\bim_offchip_CC1352R1_LAUNCHXL_nortos_ccs\Debug_unsecure\bim_offchip_CC1352R1_LAUNCHXL_nortos_ccs.hex]... J-Link: Flash download: Bank 0 @ 0x00000000: 1 range affected (8192 bytes) J-Link: Flash download: Total: 0.285s (Prepare: 0.030s, Compare: 0.079s, Erase: 0.025s, Program & Verify: 0.132s, Restore: 0.017s) J-Link: Flash download: Program & Verify speed: 61 KB/s O.K. Downloading file [.\simple_peripheral_oad_offchip_CC13X2R1_LAUNCHXL_tirtos_ccs\Release\simple_peripheral_oad_offchip_CC13X2R1_LAUNCHXL_tirtos_ccs.hex]... J-Link: Flash download: Bank 0 @ 0x00000000: 1 range affected (131072 bytes) J-Link: Flash download: Total: 1.089s (Prepare: 0.038s, Compare: 0.076s, Erase: 0.000s, Program & Verify: 0.949s, Restore: 0.025s) J-Link: Flash download: Program & Verify speed: 135 KB/s O.K. Reset delay: 0 ms Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit. Script processing completed.
Questions:
- Is there any reason explaining why downloading both binaries (bootloader.hex + firmware.out cf Test 3) does not work?
- What needs to be changed for successfully flashing the *.hex using Uniflash and Jlink?
Thanks,