Hello,
As the title suggests, I took the multi_role example (SDK: CC13x2 26x2 SDK 5.10.00.48), added another thread and used a mailbox to send data between threads. That all worked well enough, but then I wanted that the thread that posts data to the mailbox will create an event for the multi_role thread so that multi_role will check the mailbox. I tried defining the mailbox in multi_role_init and sending syncEvent to it as the event handle:
But this didn't work.
Basically I'm trying to create an API thread to receive commands over UART, which will then do certain actions in the multi_role thread. The API thread will post/read data from a mailbox and the multi_role thread will wake up and execute whatever is needed. I could simply build a clock in the multi_role thread to wake up every x amount of time and check the mailbox, but I would still rather be using events.
Any suggestions?