This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kindly suggest right Zigbee 3.0 for Gateway Application (Home/Building Automation)

Other Parts Discussed in Thread: CC2652P, SIMPLELINK-CC13X2-26X2-SDK, CC2652RB, LAUNCHXL-CC26X2R1, CC2652R, LP-CC2652RB, WL1807MOD

Hi,


We need to design the Gateway for Home/Building automation, all related requirement/feature information's are explained in the attached file, PFA FYI. You can ignore the any other modules if you feel not related to this topic, in such case, i can raise a new post for other modules.


Kindly check our requirement/application and suggest the right Zigbee 3.0 and EVM board for the same.

  • Should work with Microprocessor (Microprocessor work environment listed below, FYI)
  • Should support ZigBee 3.0 (HA 1.2)
  • Range should be maximum as possible. Kindly advise how to achieve.
  • On board PCB Antenna Sufficient or External Antenna required?



Microprocessor will be interfacing with Ethernet, WiFi, Bluetooth, Zigbee, KNX tranreceiver. and Microprocessor should have the following feature:

  • Should work with Linux OS
  • Communicate with/over BLE/BLE Mesh devices, WiFi/WiFi Mesh devices, Zigbee devices.
  • Communicate with KNX devices include Sensors, actuators, supported devices
  • Communicate over Ethernet, should support BACnet IP.
  • MQTT Client libraries and AES libraries

Security:

  • Must support secure-boot with OTPROM based core root of trust
  • Build procedure to sign the bootloader OS and application binaries with a RSA private key.
  • Secure boot verification by establishing chain of trust from OTPROM till application layer.
  • OS should be Secure Linux.
  • Storing passwords, user names, keys in a secure storage


This is one of the most important Project, We need your support to built efficient product. kindly help us.


Thanks and regards,

Naveen K

5078.Gateway Requirement.pdf