Hi
I have a application that requires to know when the SPI transfer has started. The SPI driver is in slave mode and is using a callback on CS rising to process the incoming data, this all works fine.
The application is required to notify the connected system that the SPI is busy and processing has not completed. I require to de-assert a READY signal as soon as the SPI CS falling edge is detected. When I try to configure the pin being used for SPI CS for falling edge interrupt, the SPI driver no longer works?
Does anyone know how to configure the peripheral pin so that the input interrupt can also be generated.
Thanks